About Standard Tab
Standard Tab displays the list of standard and custom tabs that are associated with the Work Queue or Unit Operations application. You can use this page to show or hide the default and custom tabs in the Work Queue or Unit Operations application. You can also specify the order in which they appear in these applications.
In this page, you can perform the following tasks:
- Show or hide the application-specific default and custom tabs.
- Change the sequence of the application-specific tabs.