About Custom Tab
Custom tabs are useful to load external third-party web applications. Using Configuration, you can add and configure (the information that will be displayed) custom tabs to Work Queue and Unit Operations applications.
Note: The external application URL must be Cross-Origin Resource Sharing (CORS)-enabled so that specified input parameters or custom properties can be transferred from the integrated application to the external application.
In this page, you can perform the following tasks:
- Create a new custom tab and associate it to either Work Queue, Unit Operations, or both the applications.
- Adding input parameters to custom tab URLs.
- Modify a custom tab.
- Delete a custom tab.