You must define your configuration in the
silentinstaller.yml file. Update the following
parameter in the silentinstaller.yml file:
Parameter
Description
WEBCLIENT_INSTALLATION_PATH: ""
Enter the Web Client Installation path in which you want to
install. For example, WEBCLIENT_INSTALLATION_PATH: "/home/
administrator/install/"
COUCHDB_SERVER: ""
Enter the Plant Applications CouchDB host name or IP
address.
COUCHDB_USERNAME: ""
Enter the CouchDB username.
COUCHDB_PASSWORD: ""
Enter the CouchDB password.
Access the utility.sh file in the
plantapps-enterprise-webclient-<buildno>
folder.
Provide execution permissions to utility.sh file by
running the following command: sudo chmod +x
your/pathto/installer/plantapps-enterprise-webclient-<buildno>/utility.sh
Run the utility.sh file by running one of the following
commands:
If you are running this utility directly on the Enterprise Edition Web Client node: <installer
path>/plantapps-enterprise-webclient-<buildno>/sudo ./utility.sh -l
-couch reset
If you are running this utility remotely on the Enterprise Edition Web Client node: <installer
path>/plantapps-enterprise-webclient-<buildno>/sudo ./utility.sh -r
-couch reset
Docker secrets are created based on the values you entered, and the
Docker stacks are redeployed so that the containers use the new
credentials.