Standard Edition Web Client Requirements
Before you begin
System Requirements
Ensure that your computer meets the system requirements as described in the following table. For more information, refer to the System Requirements section in the Plant Applications Getting Started Guide document for the latest Plant Applications release.
The Plant Application Server and Web Client servers can be hosted in the AWS/Azure Cloud. Ensure that when they are hosted in Cloud they meet the Plant Application and Web Client Server system requirements.
Item | Version |
---|---|
Operating system | 64-bit Windows 10 or Windows Server 2022 |
Couch DB server | CouchDB version 2.3.1 or 3.2.2 Note: For more information on
downloading, installing, configuring, or upgrading CouchDB,
refer to the Pre-installation Configuration (Enterprise
and Standard) section. |
Operations Hub | 2.1 with SIM3 and later, or Operations Hub 2022, 2022.4.1, or 2022.06 |
Web browsers | Chrome 107.0.5304.107 and later Devices:
Microsoft Edge v94.0.992.31 |
OLEDB Driver | Microsoft OLE DB Driver 18 for SQL Server Note: You can download the Microsoft OLE DB Driver 18 for SQL Server from the following URL: https://www.microsoft.com/en-us/download/details.aspx?id=56730. |
Hard drive | 100 GB (minimum recommended) |
Processor | 2.4 GHz clock-speed Intel Core i3, i5, or i7 CPU or
equivalent AMD Phenom CPU Note: For better performance, we
recommend to use a octa core (8-cores)
processor. |
Memory | 32 GB (minimum recommended) Note: You must have minimum 64 GB
or more if you plan to install Web Client, Historian,
Operations Hub, and Plant Applications on the same node.
However, it is recommended to install them in a distributed
environment. |
Port Requirements
This section describes the port requirements for Plant Applications Web Client. Ensure that the ports described in the following table are opened before you install Plant Applications Web Client.
To open ports on the Plant Applications Core Server, refer to the Port Requirements section in the Getting Started Guide.
Port | Description |
---|---|
15672 | The default port for the RabbitMQ Message bridge required to communicate with the Plant Applications server for retrieving data updates. |
8090/8091 | The default port for the Tomcat server. |
1433 | The default port for the Microsoft SQL server. |
9093 | The default port for Kafka. |
2185 | The default port for ZooKeeper. |
6984 | The default https port for CouchDB. |
443/5059 | The default port for Web Applications |
What to do next: Complete the pre-installation configuration, and then proceed to install the Plant Applications Standard Edition Web Client. See About Installing Standard Web Client.