About Change Data Capture (CDC)
Change Data Capture (CDC) is used to identify and track changes to data in the SQL Server database.
Plant Applications Web Client uses CDC to make the following changes available to the user immediately:
- Adding new Line and Unit which reflects in Operator app and Work-Queue app.
If the CDC is not enabled, the changes become available when the caches are refreshed after a predefined interval.
The following applications support Change Data Capture (CDC):
- Work Queue
- Route Editor
- Operator