When you install Plant Applications using Docker, both Process and Discrete services and applications are installed by default. If you have disabled the Discrete applications and want to re-enable them, perform the following two step process:
Run the utility to enable the services in the web server
Add apps in the Operations Hub
Enable the services in the web server
Procedure
Access the utility.sh in the
uc-ansible-installer folder.
Provide execution permissions to the utility.sh file by running the following command:
sudo chmod +x /uc-ansible-installer/utility.sh
Run the utility.sh by running one of the following commands:
If you want to run this utility directly on the Web Client node:
/uc-ansible-installer/sudo ./utility.sh -l
-enablediscrete reset
If you want to run this utility remotely on the Web Client node: /uc-ansible-installer/sudo ./utility.sh -r -enablediscrete reset
If you run this utility remotely, enter the details of the Web Client node.
A message appears, asking you to enter Web Client Installation Directory
Enter installation directory and then press Enter.
Re-enable apps from Operations Hub
Procedure
Access Ophub designer with Ophub tenant user credentials:
https://<ophub-host>/iqp
Select Plant Applications under Apps.
Select NAVIGATION located in the top-left corner of the screen.
Select Add new page.
Select the Discrete applications and select Add.
Now, you can access the Discrete applications in Web Client.