Legacy User Actions
Filter the Context Browser
You can filter within the Context Browser selections by asset name.
About This Task
The filter capability for the Context Browser allows you to select an asset classification via the business functional hierarchy.
During selection of an asset context, you can filter the Context Browser list by asset name.
The Context Browser contains columns of assets that are organized into business functional object groups by Enterprise, Site, Segment, and asset context groups by Asset. Each column contains asset names that can be selected and opened to select your asset. You can filter inside a column to help you find the asset context you want to use.
Procedure
Search the Context Browser
About This Task
- Enterprise
- Site
- Segment
- Asset
The Search capability of the Context Browser allows you to select an asset of interest more quickly than you would via the Context Browser hierarchy. You can select an asset name in the hierarchy to access the asset.
During selection of an asset context, you can search the Context Browser hierarchy either by asset name or asset ID.
For more information, refer to the Navigate the Asset Hierarchy section of the documentation.
Procedure
Select an Asset Context for Asset
You can use the Context Browser to select an asset context.
About This Task
For more information, refer to the Navigate the Asset Hierarchy section of the documentation.
Procedure
- In the module navigation menu, select .
- Use the Context Browser to select an asset context.
Select an Asset Context for Analysis
You can use the Context Browser to select an asset context.
About This Task
For more information, refer to the Navigate the Asset Hierarchy section of the documentation.
Procedure
- In the module navigation menu, select .
- Use the Context Browser to select an asset context.
Select an Asset Context for Dashboards
You can use the Context Browser to select an asset context.
About This Task
For more information, refer to the Navigate the Asset Hierarchy section of the documentation.
Procedure
- In the module navigation menu, select .
- Use the Context Browser to select an asset context.
Add or Remove Multiple Assets in Analysis
You can add assets for analysis within the hierarchy so that you can compare time series data for multiple assets on a chart.
About This Task
You can add the same tag for multiple assets. Adding the same tag for multiple assets allows you to compare the same tag for other assets at the same level.
You can add any asset to analysis that you have access to, enabling you to plot tags in the selected assets on the charts. This allows you to look at multiple assets to investigate or isolate an issue.
The Tag Browser and Plotted Tags sections appear in the Tag Tree Browser. The Tag Browser section lists primary and secondary assets. The primary asset is selected in the Context Browser. While you can delete secondary assets in the view, you cannot delete the primary asset.
You cannot add additional assets for Event Data Analysis charts in the Tag Tree Browser or Search Browser panes.
You can plot tags for multiple selected assets simultaneously. Assets with tag expressions plotted cannot be removed.
You can drag any tag associated with a listed asset to a chart, or remove the tag from its associated charts.
Procedure
- To add secondary assets to a chart:
- To remove a secondary asset and its associated tags:
Add Multiple Assets in Dashboards
You can add an asset context to a widget destination, allowing the user to navigate to a specified destination within Predix Essentials by selecting a link on the widget.
About This Task
Some widgets allow selection of views and multiple destinations. For more information, refer to the Navigate the Asset Hierarchy section of the documentation.
Procedure
- In the module navigation menu, select .
- Use the Context Browser to select an asset context.
- Select a view.
- In an existing card, select Action and then select Edit Card.
- Hover over a widget, and then select
.
- Configure the specific widget, as needed. For more information, refer to the Configure Widgets section of the GE Dashboards documentation.
- When you select Dashboards as the destination during configuration, select the Set Context link.
- Use the Context Browser to select a context.
- Continue the configuration for the widget.