Groups Overview

About Groups

Groups are a collection of assets or tags of the same type.

Groups are logical structures that hold instances of the same object type, and are associated to parent nodes in the business functional hierarchy.

For example, a group of asset instances cannot contain any tag instances. The group of asset instances can be associated with a segment. site, or asset instance node that is higher in the business functional hierarchy.

You can add Groups for classifications and add custom attributes for the group.

You can use Groups to locate assets or tags by the type of data provided. For instance, you can access a group of tags by function.

You can add, search and access groups by:
  • All Groups
  • Tag Classification Groups
  • Asset Classification Groups
  • Business Functional Hierarchy Groups

Predix Essentials Groups allows you to add, search, select and configure a specific group.

The Groups table lists the first 250 groups. Use the scroll bar to access additional groups.

Each specific group includes custom attributes and the objects in the group. You can add or modify custom attributes for the group. You can jump to the relevant asset or tag instance and the associated classification using links in the Objects in Group table. Objects in the group cannot be added in the user interface. For more information, refer to the related links for API and ingestion information.

Add a Group

You can add groups for classifications and instances.

About This Task

You can select the following object types when adding a group:
  • Business Functional Hierarchy Classifications
  • Asset Classifications
  • Tag Classifications
  • Business Functional Hierarchy Instances
  • Asset Instances
  • Tag Instances
Note: You cannot mix object types when creating a group.

Procedure

  1. In the module navigation menu, navigate to Assets > Groups.
  2. From the Groups page, select .
    The New Group page appears.
  3. Do the following:
    1. Enter a name for the group in the Group Name box.
    2. Enter a source ID in the Source ID box.
      Note: Entering a source ID allows you to specify a unique identifier for the new group.
    3. Enter a description for the new group in the Description box.
    4. Select an option from the Type of Objects in Group drop-down list box.
  4. Select Create.
    The new group page appears.

What To Do Next

You can now add member objects and custom attributes to the group.

Modify a Group Name

You can modify a group name.

About This Task

Group Names are visible in the Group table. Once you have selected a group in the Group table, you can modify the name. The new name for the group is propagated throughout Predix Essentials.

Procedure

  1. In the module navigation menu, navigate to Assets > Groups.
  2. Select a group link from the Groups table.
  3. In the group view, hover over, then select the group name.
  4. Enter a new name in the Group Name box, then press ENTER or select outside the field.
    The new name appears for the group on the group view.
    Note: The new group name is visible in the group view and Group table in place of the old name.

Modify a Group Description

You can modify a group description.

About This Task

Once you have selected a group in the Group table, you can modify the description. The new description for the group is propagated throughout Predix Essentials.

Procedure

  1. In the module navigation menu, navigate to Assets > Groups.
  2. Select a group link from the Groups table.
  3. On the groups view, hover over, then select the group description.
  4. Enter a new description in the Group Description box, then press ENTER or select outside the box.
    The new description appears for the group on the group view.

Delete a Group

You can remove a group and all of its member objects.

About This Task

You can select a group and remove it from the Groups table. When you remove a group, all of its member objects are also removed.

Procedure

  1. In the module navigation menu, navigate to Assets > Groups.
  2. Select a group link in the the Groups table.
    The selected group page appears.
  3. Select .
    The group and all its object members are removed.
    Important: This action cannot be undone.