Classifications Overview

About Asset and Tag Classifications

A classification is collection of asset or tag instances with common characteristics.

A classification is a modeling construct that allows a data modeler to design an asset model by identifying the common characteristics of assets or tags.

For example, suppose you have a product line of bicycles: two-wheeled, three-wheeled, and four-wheeled. The common characteristic (or attribute) for each model in the line is number of wheels. A data modeler would add this attribute to the root asset classification when the asset instances are created they will inherit the custom attribute for number of wheels. If there are additional common attributes for bicycles these can be added at the root asset classification as well.

Classifications are added to Predix Essentials during ingestion by anyone with modify asset privileges.

You can access classifications by selecting a link in an associated instance, or by searching criteria in Classifications.

Create a Classification

You can create new root-classifications or child-classifications for each level in the business functional hierarchy. You can create new root-tag classifications or child-tag classifications.

About This Task

Important: After you have created a classification, you cannot modify the placement of the classification in the business functional hierarchy. For information on deleting a classification from a Business Functional Object, refer to Delete a Classification for a Business Functional Object, and begin again.
You can create classifications in the business functional hierarchy as follows:
Table 1. Available Classification Types
Beginning from hereYou can create this type of classification
EnterpriseYou can create a root-Enterprise or a child-Enterprise.
SiteYou can create a root-Site or a child-Site.
SegmentYou can create a root-Segment or a child-Segment.
AssetYou can create root-Asset or a child-Asset.
TagYou can create a root-Tag or a child-Tag.
When you create a new classification, you must define the following:
Table 2. Classification Definitions
FieldDescription
Classification NameThe name of the new classification.
(Optional) DescriptionA description of the new classification.
Source IDA unique identifier for the new classification.
Note: You can assign same source ID to different types of classification such as Enterprise, Site, Segment, Asset, and Tag in different cases.

For example: TurbineSiteType (SiteType), turbinesitetype (AssetType), Turbinesitetype (TagType)

(Optional) Position in Hierarchy check boxCreates the new classification at the root level in the hierarchy. You can select any Type as the root. This disables the Parent Classification box.
TypeSpecifies the type of classification (Enterprise, Site, Segment, Asset, or Tag).
Parent ClassificationAllows you to define the association in which the new classification is created as a child-classification. Selecting the Parent Classification drop-down list box allows you to select from the choices available.

The Parent Classification is based on the Type selected. During creation of child-classifications, the Parent Classification created last displays by default. Otherwise, the first classification in the drop-down list box is displayed.

If the Asset or Tag Type is selected as a classification type, you can search for a classification.

Procedure

  1. In the module navigation menu, navigate to Assets > Classifications.
  2. In the classification view, select .
    Note: Classifications can be Enterprise, Site, Segment, Asset, or Tag.
    The New Classification window appears.
  3. Enter the required information in the new classification form:
    1. Enter a classification name in the Classification Name box.
    2. Optional: Enter a description for the new classification in the Description box.
    3. Enter a sourcekey for the new classification in the Source ID box.
    4. Optional: If you want the new classification to be placed into the root level of the hierarchy, select the Set as top level node check box.
      Important: Selecting this option disables the Parent Classification box.
    5. Select an option in the Type drop-down list box.
    6. If you want to change the Parent Classification, choose from the following:
      • For an Enterprise, Site, or Segment Type selection, select an option in the Parent Classification box.
      • For an Asset or Tag Type selection, select in the Parent Classification box to access the Select Classification window. Enter your search criteria, and then select Select. For more information about how to select a classification, refer to the Find and Select a Parent Classification documentation.
        Tip:
        • The Parent Classification box is disabled if the Set as top level node check box is selected.
        • The parent classifications associated with the Type selected appear as a list in the Parent Classification box by default. The Parent Classification is optionally preselected to the last created parent classification. If you are creating a classification that requires a different parent classification, you will need to change the selection.
    7. Select Create.
    Note: Create is disabled until all required fields have been completed.
    The new classification appears. The classification includes the identifier information of the classification, including any inherited attributes. Instances created using the new classification are included in the selected column in the Context Browser.

Create a Child-Classification

You can create child-classifications for each level in the business functional hierarchy. You can create new root-tag classifications or child-tag classifications.

About This Task

You can create child-classification of any type in the business functional hierarchy. The child-classification inherits all the attributes from the root-classification. The datatype defined for the attributes in the root-classification remains same and cannot be changed. However, you can add or delete custom attributes. The instances also inherit attributes from the Classification or Type under which they have been created.

For example, if an attribute Rotor Diameter within Turbine Classification is defined as integer datatype, then all the instances of the Turbine populating value for the attribute Rotor Diameter must provide integer as datatype and values must comply to the datatype.

Important: After you have created a child-classification, you cannot modify the placement of the child-classification in the business functional hierarchy. For information on deleting a classification from a Business Functional Object, refer to Delete a Classification for a Business Functional Object, and begin again.

Procedure

  1. In the module navigation menu, navigate to Assets > Classifications.
  2. In the Classification results table, select the classification from Classification Name or Parent Class for which want to add a child classification.
  3. In the selected classification view, select .
    The New Classification window appears.
  4. As needed, enter values in the available fields.
    Important: Selecting the Set as top level node check box disables the Parent Classification box and places the classification into the root level of the hierarchy.
    Note: By default, the child-classification has the same type as root-classification. However, you can change it to a different type such as Enterprise, Site, Segment, Asset, or Tag and select associated parent classification. For more information on type, refer to Create a Classification.
  5. Select Create.
    The new child-classification appears. The child-classification includes the identifier information of the classification, including any inherited attributes. The custom attributes from the root-classification are copied to the inherited attributes in the child-classification. You can add more custom attributes in the child-classification; however, the attribute name cannot be same as the existing inherited attributes. Instances created using the new child-classification are included in the selected column in the Context Browser.

Find and Select a Parent Classification

You can search for a specific Asset or Tag classification to use as a parent classification.

About This Task

After selecting Asset or Tag as the Type while creating a classification, you can search for a parent classification to associate with the new classification.
Note: Searching for a classification is only available if you have selected Asset or Tag as the Type while creating a classification. For more information, refer to the Creating a Classification in the Business Functional Hierarchy documentation.
The following search parameters are supported for asset or tag types:
  • uri
  • name
  • sourcekey
  • description
  • attributes
  • reservedattributes
  • parent

Procedure

  1. In the module navigation menu, navigate to Assets > Classifications.
  2. In the classification view, select .
    The New Classification page appears.
  3. Enter the required information. For more information about how to do this, refer to the Create a Classification in the Business Functional Hierarchy documentation.
  4. In the New Classification page, select Asset or Tag in the Type box.
  5. Select in the Parent Classification box to access the Select Classification window.
  6. Enter a search string using modifiers and wild cards, and then press ENTER to activate the search string.
  7. Scroll through the results, select an option from the list, then select Select.
    The selected classification appears in the Parent Classification box.
  8. Select Create.
    The new classification appears. The classification includes the identifier information of the classification, including any inherited attributes. Instances created using the new classification are included in the selected column in the Context Browser.

Add Members to a Classification Group

You can add member objects to an existing classification group.

About This Task

You can select classification member objects and specify an existing group for which to add the selected members.

Procedure

  1. In the module navigation menu, navigate to Assets > Classifications.
  2. Search for a classification type.
    The selected classification items appear in the Classifications table.
  3. Scroll through the items in the table, and select check boxes in the Selected column for the items you want to add to a group.
    Alternatively, you can select the Select All check box to add all the items to a group.
  4. Select Add to Group.
    The Add to Group page appears.
  5. Enter criteria for a group name or source ID into the Search box, then select Search.
  6. Select a group from the list and select Add.
    The member objects are added to the selected group.

Modify a Classification Name

You can modify a classification name.

About This Task

Once you have selected a classification in the Classifications results table, you can modify the name. The new name for the asset or tag classification is propagated throughout Predix Essentials.

Procedure

  1. In the module navigation menu, navigate to Assets > Classifications.
  2. Find and select a Classification Name or Parent Class link in the Classifications results table.
  3. On the selected classification view, hover over, then select the classification name.
  4. Enter a new name in the Classification Name box, then press ENTER or select outside the field.
    The new name appears for the classification on the selected view and on the Classification results table.

Modify a Classification Description

You can modify a classification description.

About This Task

Once you have selected a classification in the Classifications results table, you can modify the description. The new description for the classification is propagated throughout Predix Essentials.

Procedure

  1. In the module navigation menu, navigate to Assets > Classifications.
  2. Find and select a classification in the Classifications results table.
  3. Select a Classification Name or Parent Class link from the Classifications results table.
  4. In the selected classification view, hover over, then select the classification description.
  5. Enter a new description in the Classification Description box, then press ENTER or select outside the box.
    The new description appears for the classification on the selected view and on the Classification results table.

Delete a Classification for a Business Functional Object

You can delete a business functional object classification from Predix Essentials.

About This Task

A business functional object refers to the Enterprise, Site, and Segment locations within the business functional hierarchy.

You can delete a business functional object classification if it does not have any child-classifications or associated asset or tag instances.
Tip:
  • Deleting a classification cannot be undone.
  • You must delete any associated child-classifications and asset or tag instances before you can delete a business functional object classification.

Procedure

  1. In the module navigation menu, navigate to Assets > Classifications.
  2. Select an Enterprise Classification, Site Classification, or Segment Classification from the Classification Type drop-down list box.
  3. Apply other filters as needed, then select Apply.
  4. In the Classification results table, hover over and select for the classification you want to delete.
    Tip: Alternatively, you can select the classification link and delete the classification using in the classification view.
  5. Select Delete in the confirmation window to delete the classification.
    The business functional object classification is permanently removed from the database.
    Note:
    • Deleting a business functional object classification permanently deletes the classification, all attributes, configuration, history information and membership in groups.
    • If you are attempting to delete a business functional object classification with associated child-classifications or asset or tag instances, an error message appears and the business functional object classification is not deleted.

Delete an Asset or Tag Classification

You can delete an asset or tag classification from Predix Essentials.

About This Task

You can delete an asset classification if it does not have any child-classifications or associated asset instances. You can delete a tag classification if it does not have any associated tag instances.
Tip:
  • Deleting a classification cannot be undone.
  • You must delete any associated child-classifications and asset instances before you can delete an asset classification.
  • You must delete any associated tag instances before you can delete a tag classification.

Procedure

  1. In the module navigation menu, navigate to Assets > Classifications.
  2. Find and select an Asset Classification or Tag Classification on the Classifications results table.
  3. On the asset or tag classification view, select in the view.
    Tip: Alternatively you can delete a classification directly from the the Classifications results table by hovering over the classification and selecting .
  4. Select Delete in the confirmation window to delete the asset or tag classification.
    The asset or tag classification is permanently removed from the database.
    Note:
    • Deleting an asset or tag classification permanently deletes the classification, all attributes, configuration, history information and membership in groups.
    • If you are attempting to delete an asset classification with associated child-classifications or asset instances, an error message appears and the asset classification is not deleted.
    • If you are attempting to delete a tag classification with associated tag instances, an error message appears and the tag classification is not deleted.