Installation

System Requirements

Supported Operating Systems

The following table lists the operating systems and corresponding versions that the Rounds Pro mobile app supports.

Operating SystemVersion(s) Supported
iOS15, 16 and 17 (Recommended)
Android12, 13 and 14(Recommended)
WindowsWindows 10 (64 bit)
Note: The method used to access Reference Documents in the Rounds Pro mobile app will vary depending on your device platform. For example, on Windows and Android devices, the first time you access Reference Documents, you will be prompted to select the application in which you want to open a file, and this selection will then become the default. Apple iOS will always prompt you to select an application.

Installation Pre-requisites

  • Any management policy applied to mobile devices must be set up to allow the required permissions for the Rounds Pro mobile app mobile application. If restrictions are placed on iOS, Windows, or Android devices by a global policy or mobile device management system, device storage, scanning, photography, location services, and other functionality may be disabled.
  • If you are using a Windows device, ensure that Windows App Store access is enabled.
  • Ensure that the application is distributed to all relevant devices.

Install the Rounds Pro mobile app on an iOS Device

Before You Begin

If you are deploying the Rounds Pro mobile app to manage iOS devices via a Mobile Device Management (MDM) solution, you can configure the server and datasource/tenant settings before deploying the app. To do so, modify the plist file as follows, and use it in the MDM solution:
<?xml version="1.0" encoding="UTF-8"?>
<!DOCTYPE plist PUBLIC "-//Apple//DTD PLIST 1.0//EN" "http://www.apple.com/DTDs/PropertyList-1.0.dtd">
<plist version="1.0">
<dict>
	<key>serverURL</key>
	<string><your server URL></string>
	<key>tenantID</key>
	<string><your tenant/datasource ID></string>
</dict>
</plist>
After you configure, the Server Settings page that first appears is automatically populated with the specified URL and tenant/datasource details, and you will be automatically directed to the login page.

Procedure

  1. Access the Rounds Pro mobile app from the App Store.
    Note: If manually searching the App Store, enter GE Digital APM Rounds Pro.
  2. Download the Rounds Pro mobile app to your device.
    The Rounds Pro mobile app is installed on your device.

Results

The Rounds Pro mobile app is downloaded from the App Store and installed on your iOS device.

Install the Rounds Pro mobile app on an Android Device

Before You Begin

If you are deploying the Rounds Pro mobile app to manage Android devices via a Mobile Device Management (MDM) solution, you can configure the following settings before deploying the app:
  • serverURL: Enter the fully qualified path to the APM server (https://<server name>.com/meridium).
  • tenantID: Enter the tenant or datasource ID.
After you configure, the Server Settings page that first appears is automatically populated with the specified URL and tenant/datasource details, and you will be automatically directed to the login page.

Procedure

  1. Access the Rounds Pro mobile app from the Google Play Store.
    Note: If manually searching the Google Play Store, enter GE Digital APM Rounds Pro.
  2. Download the Rounds Pro mobile app to your device.
    The Rounds Pro mobile app is installed on your device.

Results

The Rounds Pro mobile app is downloaded from the Google Play Store and installed on your Android device.

Install the Rounds Pro mobile app on a Windows Device from App store

Procedure

  1. Access the Rounds Pro mobile app from the Windows App Store.
    Note: If manually searching the App Store, enter GE Digital APM Rounds Pro.
  2. Download the Rounds Pro mobile app to your device.
    The Rounds Pro mobile app is installed on your device.

Results

The Rounds Pro mobile app Windows application can be downloaded from the Windows App store and installed on your Windows device.

Install the Rounds Pro mobile app on a Windows Device

Before You Begin

Important:
  • Before installing the Rounds Pro mobile app, the Developer mode needs to be activated in the Update & Security settings. To activate the developer mode, in the Update & Security page, select For developers and then in the Use developer features section, select Developer mode.

Procedure

  1. On the device on which you want to install the Rounds Pro mobile app, extract the content of the application package file to a local folder.
  2. In the folder into which you extracted the application package file content, navigate to the folder path MobileAPM.UWP\AppPackages\MobileAPM.UWP_<version>_Test containing the Install.ps1 file.
  3. Right-click on the Install.ps1, and then select Run with PowerShell.
    The installation process starts. A message may appear prompting you to install a certificate.
    Note: If you already have the certificate installed as part of previous installation, you will not see the prompt.
  4. Select Yes.
    The installer resumes the installation of the application and installs the dependencies. The Rounds Pro mobile app is installed on the Windows device for all the current and future Windows user accounts.
  5. Optional: To cancel future installations or uninstall the Rounds Pro mobile app, in the folder into which you extracted the application package file content, right-click Uninstallation file name, and then select Run as an Administrator.
    Note: If you are using a touch-screen device, press and hold Uninstallation file name, and then select Run as an Administrator.
    The Rounds Pro mobile app is uninstalled for the Windows user account that is currently logged in, and installations for future Windows user accounts are cancelled.

Results

The Rounds Pro mobile app is installed on your Windows device.