Enumeration Event Types
Event Types have a limited/defined set of named values, means each value has a numeric
value and a textual name. The predefined enumeration event type set which comes with the
MTConnect server installation includes all enumeration event types defined in MTConnect
Standard version 1.4. The complete list of the predefined enumeration event types you
can find in topic Supported MTConnect Standard.
Type Name
The name of the event type as defined in the MTConnect standard. This name must match exactly the type name in the MTConnect standard. If a type has one or multiple sub types, then multiple entries have to be defined, one for each type/sub type pair.
Sub Type Name
The name of the event sub type as defined in the MTConnect standard. This name must match exactly the type name in the MTConnect standard. If no sub type is specified in the MTConnect standard then this field has to be empty.
Enum Type Name
Depending on the possible named values of the enumeration event type, a predefined enumeration type can be selected for the event type. The selected enumeration type has to contain all possible name-value pairs the enumeration event can take-on. The complete list of the predefined enumeration types and their name-value pairs you can find in topic Supported MTConnect Standard.