Create a Recommendation from an Alert on a Windows Mobile Device

Steps

  1. On the Windows Mobile device, access the Readings - Alert screen.
  2. If you enter a reading value that has been configured in the GE Digital APM Framework application to trigger an alert, when you try to navigate away from that checkpoint on the Windows Mobile Device, the Readings - Alert screen will appear.
  3. On the Readings - Alert screen, select .

    The New Recommendation screen appears.

    The following text boxes are populated automatically with values from the reading:

    If the Measurement Location record that is associated with this Operator Rounds Recommendation record contains a value in the Asset Description box, that value will appear below in the Asset ID box.

    The Headline box contains the value you entered for the reading, followed by:

  4. In the Description box, enter a description of the recommendation.

    Note: If you entered text in the Description box on the Readings - Detail screen, that text will appear in the Description field on the Recommendations screen. You can modify the description on this screen, and the updated text will be displayed when you return to the Readings - Detail screen.

  5. In the Priority list, select a priority for the recommendation. You can select: High, Medium or Low.

  6. Select Save.

    The recommendation is saved, and the Readings - Alert screen returns to focus.

Copyright © 2018 General Electric Company. All rights reserved.