The Rounds module provides users with the capability to manage route-based, recurring tasks such as operator checks, routine maintenance, lubrication tasks, safety inspections, etc. The module includes two main features: route design and data collection.
The route design feature enables analysts to define the checkpoints (e.g., measurements to be taken, tasks to be completed, etc.) for each asset, and arrange them into routes. Checkpoints can be scheduled individually, or the entire route can be scheduled. Checkpoints can be defined as part of the asset strategy using the Asset Strategy Management module, or created within the route designer based on templates and template groups.
Note: Checkpoints include both Measurement Locations and Lubrication Requirements. Wherever Checkpoint is used, both Lubrication Requirements and Measurement Locations are assumed to be included.
Copyright © 2018 General Electric Company. All rights reserved.