Steps
In the left pane, select Performance & Reports.
The Performance & Reports workspace appears. The Performance Records tab is selected by default, displaying a list of Performance records associated with the GAA Unit for the current year in reverse chronological order.
The Performance Records section contains the following columns of information:
Record ID: Contains links to access the Performance records associated with the selected Primary Event, for the specified month.
The link to the Performance record appears in the following format:
<Record Name> ~ <Record Type> ~~ <Performance Type>
Note: As needed, you can modify the ID Template of the GAA Configuration family to specify a different format.
<Performance Type> indicates one of the following:
Event List: Contains the number of events that occurred during the specified month and the number of events that are in OUT OF SYNC status currently. When you select the link in this column, you can view the list of events that occurred during the specified month. The events that are in SYNCED status appear with a green bar to their left, and the events that are in the OUT OF SYNC status appear with a red bar to their left.
Sync Status: Indicates whether or not the Performance record includes updated information. A Performance record can have one of the following statuses:
Note: If no Performance record exists for the specified month, you can create a Performance record for that month. You can create a Performance record that includes all events, or a Performance record that includes all events except the OMC events.
Tip: You can also select
The Records for the Year option allows you to specify the year for which you want to view the Performance records in the Performance Records section. By default, current year is selected.
In the month for which you want to view a Performance record, select the link.
On a new page, the following tabs appear:
Notes: As needed, you can modify the values in the available fields, and then select
Copyright © 2018 General Electric Company. All rights reserved.