The Performance & Reports workspace appears, displaying the Performance Records section, which contains a list of Performance records associated with the GAA Unit for the current year.
For the month for which you want to create a Performance record, in the Sync Status column, select Create Record.
Note: You can create a Performance record for a month only if no Performance record exists for that month. If a Performance record exists for a month but is in OUT OF SYNC status, you can regenerate the Performance record for that month.
Note: For GAA Units for which the value in the Primary Regulatory Organization field is Canadian Electricity Association (CEA), the NERC Event Types mapped to the CEA Event Types are used to calculate data. The calculations are based on the calculations defined for North American Reliability Corporation (NERC) in the IEEE Standard Definitions for Use in Reporting Electric Generating Unit Reliability, Availability, and Productivity documentation.
If you want to include the calculated values, then, in the upper-right corner of the Performance Records section, select .
The Regenerate Record dialog box appears, asking you to confirm that you want to regenerate the Performance record.
Select Yes.
The Performance record appears in the workspace. The Sync Status column indicates that the record is in SYNCED status.
The Performance & Reports workspace appears, displaying the Performance Records section, which contains a list of Performance records associated with the GAA Unit for the current year.
In the upper-left corner of the Performance records section, select .
The Records for the Year window appears.
Select the year for which you want to generate the Performance records, and then select Apply.
The Performance records associated with the GAA Unit for the selected year appear.
In the upper-right corner of the Performance Records section, the button is enabled.
Note: If all the Performance records for the year exist, the button is disabled.
Select .
The Performance for <Year> dialog box
appears, asking you to confirm that you want to create and regenerate the Performance records for the selected year.
Select Yes.
The Performance records for the selected year are created and regenerated. If the regeneration of the Performance records was successful, the status will be SYNCED. If the regeneration was unsuccessful, the status will be OUT OF SYNC.
If an error occurred while creating and regenerating Performance records, the button will appear. If you want to view the details of the error, select .
Note: Performance records that were previously created within the same year will not be automatically regenerated. You will need to regenerate each record.
If the Primary Event is spread across months, the Event Start Date and Event End Date fields contain different months. When the performance calculation is run for all these months, the Event will be included in the performance calculation for each month. In this scenario, in the Event List column, the total number of events will be displayed accordingly.