GAA Performance Summary records store information about the fields that are defined for the GAA Performance Summary family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the GAA Performance Summary family and appear on the datasheet. The information in the table reflects the baseline state and behavior of these fields. The values in these fields are defined by NERC in the GADS DRI. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Note: Wherever we refer to the unit, we mean the unit represented by the GAA Unit record to which the Performance record is linked.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Actual Unit Starts | Numeric | Indicates the number of actual times the unit started within a given month and year. |
This field is disabled and is populated automatically when the value in the Reporting Status field is set to Unit Level Approval, validation is performed on this field to ensure that the value is equal to the number of Attempted Unit Starts minus the number of Startup Failures. This field is required. |
Attempted Unit Starts | Numeric | Indicates the number of attempted starts for the unit within a given month and year. |
This field is disabled and is populated automatically when the value in the Reporting Status field is set to Unit Level Approval, validation is performed on this field to ensure that the value is equal to the number of outage events that occurred within the month that the Performance record represents. This field is required. |
Available Hours | Numeric |
Indicates the total number of hours in which the unit was available. |
This field is disabled and populated automatically as the sum of Pumping Hours, Reserve Shutdown Hours (RSH), Service Hours (SH), and Synchronous Condensing Hours. This field is required. This value is defined by NERC in the GADS DRI and included in NERC performance reports. |
Availability Factor | Numeric | Indicates the fraction of a given operating period in which a Generating Unit is available without any outages |
This field is disabled and populated automatically using the following formula: (Available Hours / Period Hours) × 100% This value is defined by NERC in the GADS DRI. |
Average Run Time | Numeric | Indicates the average number of hours a unit runs and produces power. |
This field is disabled and populated automatically using the following formula: (Service Hours / Actual Unit Starts ) × 100% This value is defined by NERC in the GADS DRI. |
Extension of Scheduled Outage Hours
|
Numeric |
Indicates the number of hours that the unit was scheduled to be inactive. |
This field is disabled and populated automatically as the sum of Planned Extension Outage Hours and Maintenance Extension Outage Hours. This field is required. |
Forced Outage Hours | Numeric | Indicates the number of hours the unit was inactive due to immediate, delayed, and postponed outages and startup failure outages. |
This field is disabled and populated automatically as the sum of all hours experienced during Forced Outages (U1, U2, U3) and Startup Failures (SF). This field is required. |
Forced Outage Factor | Numeric | Indicates the fraction of a given operating period in which a Generating Unit is not available due to forced outages. |
This field is disabled and populated automatically using the following formula: (Forced Outage Hours / Period Hours) × 100% This value is defined by NERC in the GADS DRI. |
Forced Outage Rate | Numeric | A measure of the probability that a GAA Unit will not be available due to forced outages. |
This field is disabled and populated automatically using the following formula: [Forced Outage Hours / ∑ (Service Hours + Synchronous Hours + Pumping Hours)] × 100% This value is defined by NERC in the GADS DRI. |
Forced Outage Rate Demand | Numeric | A measure of the probability that a GAA Unit will not be available due to forced outages when there is demand on the unit to generate. |
This field is disabled and populated automatically using the following formula: [Forced Outage Hours Demand / (Σ Forced Outage Hours Demand + Service Hours)] × 100% This value is defined by NERC in the GADS DRI. |
Gross Actual Generation (G) | Numeric |
Indicates the actual gross generation of the unit during the month for which the Performance record stores generation data. |
This field is disabled and populated automatically using the following formula: Gross Actual Generation = Max Generation (G) - Unavailable Generation Where,
This field is used to calculate the value in the Gross Generation of Electricity field in the GAA Fuel Report records that are linked to the Performance record. This field accepts both positive and negative numbers. In some cases, if a unit does not produce power during the month, the equipment in the plant still consumes power, causing a negative Gross Actual Generation value. This field becomes required when the value in the Reporting Status field is set to Unit Level Approval. This value is defined by NERC in the GADS DRI and included in NERC performance reports. |
Gross Dependable Capacity (G) | Numeric | Indicates the gross dependable capacity of the unit. |
This field is populated automatically with the value in the Gross Dependable Capacity field in the Unit Capacity record for a GAA Unit based on the start date of the Performance record. This value is defined by NERC in the GADS DRI and included in NERC performance reports. If you modify the value in this field, a validation message appears indicating that the pumping hours or capacity values have changed and that the performance calculation is being run. |
Gross Maximum Capacity (G) | Numeric | Indicates the gross maximum capacity of the unit during the month for which the Performance record stores generation data. |
This field is populated automatically with the value in the Gross Maximum Capacity field in the Unit Capacity record for a GAA Unit based on the start date of the Performance record. This value is defined by NERC in the GADS DRI and included in NERC performance reports. If you modify the value in this field, a validation message appears indicating that the pumping hours or capacity values have changed and that the performance calculation is being run. |
Inactive Hours | Numeric |
Indicates the number of hours the unit was inactive during the month for which the Performance record stores generation data. |
This field is disabled and populated automatically with the value from the Event Duration field in the Primary Event record that is linked to the Performance record. This field is populated automatically as the sum of durations of Inactive events (IR, MB, RU). This field is required. This value is defined by NERC in the GADS DR. |
Maintenance Outage Hours | Numeric |
Indicates the number of hours the unit was inactive due to maintenance outages. |
This field is disabled and populated automatically as the sum of all hours that occurred during Maintenance Outages (MO) and Maintenance Outage Extensions (ME) of any Maintenance Outages (MO). This field is required. |
Maintenance Outage Factor | Numeric | Indicates the fraction of a given operating period in which a Generating Unit is not available due to maintenance outages. |
This field is disabled and populated automatically using the following formula: (Maintenance Outage Hours / Period Hours) × 100% This value is defined by NERC in the GADS DRI. |
Max Generation (G) | Numeric |
Indicates the maximum gross generation that the unit is capable of producing during the month for which the Performance record stores generation data. |
This field is disabled and populated automatically using the following formula: Max Generation (G) = Period Hours × Gross Max Capacity |
Max Generation (N) | Numeric |
Indicates the maximum net generation that the unit is capable of producing during the month for which the Performance record stores generation data. |
This field is disabled and populated automatically using the following formula: Max Generation (N) = Period Hours × Net Max Capacity |
Mean Forced Outage Duration | Numeric | Indicates the average number of hours a unit is unproductive because of forced outage. |
This field is disabled and populated automatically using the following formula: Forced Outage Hours which occur from in-service state only / Number of Forced Outages which occur from in-service state only This value is defined by NERC in the GADS DRI. |
Mean Maintenance Outage Duration | Numeric | Indicates the average number of hours a unit is unproductive because of maintenance outage. |
This field is disabled and populated automatically using the following formula: Forced Outage Hours which occur from in-service state only / Number of Maintenance Outages which occur from in-service state only This value is defined by NERC in the GADS DRI. |
Mean Planned Outage Duration | Numeric | Indicates the average number of hours a unit is unproductive because of planned outage. |
This field is disabled and populated automatically using the following formula: Planned Outage Hours which occur from in-service state only / Number of Planned Outages which occur from in-service state only This value is defined by NERC in the GADS DRI. |
Mean Service Time to Forced Outages | Numeric | Index representing mean service time to in-service forced outages. |
This field is disabled and populated automatically using the following formula: Service Hours / Number of (Unplanned) Forced Outages which occur from in-service state only This value is defined by NERC in the GADS DRI. |
Mean Service Time to Maintenance Outage | Numeric | Index representing mean service time to in-service maintenance outages. |
This field is disabled and populated automatically using the following formula: Service Hours / Number of Maintenance Outages which occur from in-service state only This value is defined by NERC in the GADS DRI. |
Mean Service Time to Planned Outage | Numeric | Index representing mean service time to in-service planned outages. |
This field is disabled and populated automatically using the following formula: Service Hours / Number of Planned Outages which occur from in-service state only This value is defined by NERC in the GADS DRI. |
Mean Service Time to Unplanned Outage | Numeric | Index representing mean service time to in-service unplanned outages. |
This field is disabled and populated automatically using the following formula: Service Hours / Number of Unplanned Outages which occur from in-service state only This value is defined by NERC in the GADS DRI. |
Mean Unplanned Outage Duration | Numeric | Indicates the average number of hours a unit is unproductive because of unplanned outage. |
This field is disabled and populated automatically using the following formula: Unplanned Outage Hours which occur from in-service state only / Number of Unplanned Outages which occur from in-service state only This value is defined by NERC in the GADS DRI. |
Net Actual Generation (N) | Numeric |
Indicates the actual net generation of the unit during the month for which the Performance record stores generation data. |
This field is disabled and populated automatically using the following formula: Net Actual Generation = Max Generation (N) - Unavailable Generation Where,
This field is used to calculate the value in the Net Generation of Electricity field in the Generation Fuel Report records that are linked to the Performance record. This field accepts both positive and negative numbers. In some cases, if a unit does not produce power during the month, the equipment in the plant still consumes power, causing a negative Net Actual Generation value. This field becomes required when the value in the Reporting Status field is set to Unit Level Approval. This value is defined by NERC in the GADS DRI and included in NERC performance reports. |
Net Dependable Capacity (N) | Numeric |
Indicates the net dependable capacity of the unit. |
This field is populated automatically with the value in the Net Dependable Capacity field in the Unit Capacity record for a GAA Unit based on the start date of the Performance record. This field is required. This value is defined by NERC in the GADS DRI and included in NERC performance reports. If you modify the value in this field, a validation message appears indicating that the pumping hours or capacity values have changed and that the performance calculation is being run. |
Net Maximum Capacity (N) | Numeric | Indicates the net maximum capacity of the unit during the month for which the Performance record stores generation data. |
This field is populated automatically with the value in the Net Maximum Capacity field in the Unit Capacity record for a GAA Unit based on the start date of the Performance record. This field is required. This value is defined by NERC in the GADS DRI and included in NERC performance reports. If you modify the value in this field, a validation message appears indicating that the pumping hours or capacity values have changed and that the performance calculation is being run. |
Number of Forced Outages | Numeric | Indicates the number of times the unit is inactive due to Forced Outages when the unit is in in-service state. | This field is disabled and populated automatically when each time the state of the unit changes from In-service to Forced Outage, this field is incremented by 1. |
Number of Maintenance Outages | Numeric | Indicates the number of times the unit is inactive due to Maintenance Outages when the unit is in in-service state. | This field is disabled and populated automatically when each time the state of the unit changes from In-service to Maintenance Outage, this field is incremented by 1. |
Number of Non Curtailing Events |
Numeric |
Indicates the number of Non Curtailing events that occur in a Unit during the specified month. |
This field is disabled and populated automatically when each time an Event occurs with value in the Capacity Event Type field specified as NC (Noncurtailing Event), this field is incremented by 1. |
Number of Planned Outages | Numeric | Indicates the number of times the unit is inactive due to Planned Outages when the unit is in the in-service state. | This field is disabled and populated automatically when each time the state of the unit changes from In-service to Planned Outage, this field is incremented by 1. |
Number of Unplanned Outages | Numeric | Indicates the number of times the unit is inactive due to Unplanned Outages when the unit is in the in-service state. | This field is disabled and populated automatically when each time the state of the unit changes from In-service to Unplanned Outage, this field is incremented by 1. |
Period Hours | Numeric | Indicates the number of hours the unit was active during the month for which the Performance record stores generation data. |
This field is disabled and populated automatically. The value in this field is equal to the sum of the values in the Available Hours field and Unavailable Hrs field. This field is required. |
Plant ID | Character | Identifies the plant in which the unit resides. | This field is disabled and populated automatically with the value in the Plant ID field in the GAA Plant record. The GAA Plant record is linked to the GAA Unit record for an existing Performance record. |
Plant Name | Character | Identifies the name of the plant in which the unit resides. | This field is disabled and populated automatically with the value in the Plant Name field in the GAA Plant record. The GAA Plant record is linked to the GAA Unit record for an existing Performance record. |
Planned Outage Hours | Numeric |
Indicates the number of hours the unit was inactive due to planned outages. |
This field is disabled and populated automatically as the sum of all hours experienced during Planned Outages (PO) and Planned Outage Extensions (PE) of any Planned Outages (PO). This field is required. |
Planned Outage Factor | Numeric | Indicates the fraction of a given operating period in which a Generating Unit is not available due to planned outages. |
This field is disabled and populated automatically using the following formula: (Planned Outage Hours / Period Hours ) × 100% This value is defined by NERC in the GADS DRI. |
Primary Unit Code | Character | Indicates the unit represented by the GAA Unit record to which the Performance record is linked. |
This field is disabled and populated automatically with the value in the Primary Unit Code field in the GAA Unit record that is linked to a Performance record. This field is required. This value is defined by NERC in the GADS DRI and included in NERC performance reports. |
Primary Utility Code | Character | Indicates the utility under which the unit represented by the GAA Unit to which the Performance record is linked operates. |
This field is disabled and populated automatically with the value in the Primary Utility Code field in the GAA Unit record. This field is required. This value is defined by NERC in the GADS DRI and included in NERC performance reports. |
Pumping Hours | Numeric | Indicates the number of hours the unit operated as a pump. |
This field is enabled in Performance records that contain the value Pumped Storage/Hydro in the Unit Type field. You can enter a value in this field manually. This field is required. This value is defined by NERC in the GADS DRI. If you modify the value in this field, a validation message appears indicating that the pumping hours or capacity values have changed and that the performance calculation is being run. |
Reporting Date | Date | Indicates the date on which the Performance record was approved and reported. |
This field is populated automatically with the date when the record was created. This field is disabled when the Performance record is in the Approved state. This field is required. |
Reporting Month | Character | Indicates the month that the Performance record represents. |
The combination of the value in this field and the Reporting Year field represents a unique year and month combination. You can create only one record with this combination for a particular type of Performance. This field is disabled and populated automatically with the month when the record was created. This value is included in NERC performance reports. |
Reporting Year | Numeric |
Indicates the year that the Performance record represents. |
The combination of the value in this field and the Reporting Month field represents a unique year and month combination. You can create only one record with this combination for a particular type of Performance. This field is disabled and populated automatically with the year of the created record. This value is included in NERC performance reports. |
Reserve Shutdown Hours | Numeric | Indicates the sum of all the hours that the unit was available, but was not in service. |
This field is disabled and populated automatically as the sum of all hours the unit was not in service. This field is required. |
Revision | Numeric | Indicates the revision number of the Performance record. |
You must increment this number each time you resubmit a report which includes information in the Performance record to NERC or CEA. This value is defined by NERC in the GADS DRI. |
Scheduled Outage Hours | Numeric | Indicates the number of hours that the unit was scheduled to be inactive. |
This field is disabled and populated automatically with the sum of all hours experienced during Planned Outages (PO), Maintenance Outages (MO), and Scheduled Outage Extensions (PE and ME) of any Maintenance Outages (MO) and Planned Outages (PO). This value is defined by NERC in the GADS DRI. |
Scheduled Outage Factor | Numeric | Indicates the fraction of a given operating period in which a Generating Unit is not available due to scheduled outages. |
This field is disabled and populated automatically using the following formula: (Scheduled Outage Hours / Period Hours) × 100% This value is defined by NERC in the GADS DRI. |
Service Factor | Numeric | Indicates the fraction of service hours to period hours in a given operating period. |
This field is disabled and populated automatically using the following formula: (Service Hours / Period Hours) × 100% This value is defined by NERC in the GADS DRI. |
Start Reliability | Numeric |
Indicates the starting reliability of the unit. |
This field is disabled and populated automatically using the following formula: (Actual Unit Starts / Attempted Unit Starts)*100 |
Synchronous Condensing Hours | Numeric |
Indicates the number of hours the unit operated in synchronous condensing mode. |
This field is disabled and populated as the sum of durations of Non-Curtailing events when cause code of the event is 9340 Synchronous Condenser Operation. This value is defined by NERC in the GADS DRI. |
Typical Unit Loading Characteristics |
Numeric | Indicates the time during which the unit was responsible for generating power. |
This field is populated automatically with the value in the Default Unit Loading field in the GAA Unit record to which the Performance record is linked. This value is defined by NERC in the GADS DRI. |
Unit ID | Character | Identifies the unit. | This field is disabled and populated automatically with the value in the Unit ID field in the GAA Unit record that is linked to a Performance record. |
Unit Name | Character | Identifies the name of the unit. | This field is disabled and populated automatically with the value in the Unit Name field in the GAA Unit record in an existing Performance record. |
Unavailable Hours | Numeric |
Indicates the number of hours that the unit was unavailable. |
This field is disabled and populated automatically as the sum of the Forced Outage Hours (FOH), Maintenance Outage Hours (MOH), and Planned Outage Hours (POH). This value is included in NERC performance reports. |
Unplanned Outage Hours | Numeric | Indicates the number of hours that the unit was inactive due to unscheduled outages. | This field is disabled and populated automatically with the sum of all hours experienced during Forced Outages (U1, U2, U3), Startup Failures (SF), Maintenance Outages (MO), and Maintenance Outage Extensions (ME) of any Maintenance Outages (MO). |
Unit Type | Character | Identifies the type of the unit. | This field is disabled and populated automatically with the value in the GADS Unit Type field in the GAA Unit record that is linked to a Performance record. |
Unavailability Factor | Numeric | Indicates the fraction of a given operating period in which a Generating Unit is not available due to outages. |
This field is disabled and populated automatically using the following formula: (Unavailable Hours / Period Hours) × 100% This value is defined by NERC in the GADS DRI. |
Unplanned Outage Factor | Numeric | Indicates the fraction of period a Generating Unit is not available due to unplanned outages. |
This field is disabled and populated automatically using the following formula: (Unplanned Outage Hours / Period Hours ) × 100% This value is defined by NERC in the GADS DRI. |
Verbal Description | Character | Indicates additional information about the GAA Unit record that is linked to the Performance record. |
You can manually enter the description in this field. When you create a Performance record, you can enter a verbal description of up to 255 characters. When you generate a NERC Performance Report, the verbal description in the generated report will display only the first 50 characters of the description that you entered in the Verbal Description field. |
Copyright © 2018 General Electric Company. All rights reserved.