GAA Unit Capacity records store information about the fields that are defined for the GAA Unit Capacity family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the GAA Unit Capacity family and appear in the Information section of the GAA Unit Capacity datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
End Date | Date | Identifies the end date till when the Unit Capacities will be applicable on the GAA Unit. | If no End Date is defined in a GAA Unit Capacity record, the Start Date of the next GAA Unit Capacity record will be considered as the End Date for this GAA Unit Capacity record. |
Entity ID | Character |
Identifies the GAA Unit Capacity record. |
This field is populated using the following format: <UnitID> ~ <StartDate> ~ <EndDate> Where,
|
Gross Dependable Capacity | Numeric | Identifies the gross dependable electrical generation capacity of the GAA Unit during the specified period. |
The value in Gross Dependable Capacity field must be less than the value in Gross Maximum Capacity field. |
Gross Maximum Capacity | Numeric | Identifies the gross maximum electrical generation capacity of the GAA Unit during the specified period. |
You must provide a value in this field or the Net Maximum Capacity field. This field is required if you do not provide a value in the Net Maximum Capacity field. The value in Gross Maximum Capacity field must be greater than the value in Net Maximum Capacity field. |
Net Dependable Capacity | Numeric | Identifies the net dependable electrical generation capacity of the GAA Unit during the specified period. |
The value in Net Dependable Capacity field must be less than the value in Net Maximum Capacity field. |
Net Maximum Capacity | Numeric | Identifies the net maximum electrical generation capacity of the GAA Unit during the specified period. |
You must provide a value in this field or the Gross Maximum Capacity field. This field is required if you do not provide a value in the Gross Maximum Capacity field. The value in Net Maximum Capacity field must be less than the value in Gross Maximum Capacity field. |
Start Date | Date | Identifies the start date when the Unit Capacities will be applicable on the GAA Unit. |
The Start Date of any GAA Unit Capacity record must be a date after the End Date of the previous GAA Unit Capacity record. When you add a GAA Unit record, a GAA Unit Capacity record is automatically created with the values defined in the capacity related fields in the GAA Unit record. In the default GAA Unit Capacity record, the Start Date is set to 01/01/1900 00:00:00 and the End Date is blank. If you want to add an additional GAA Unit Capacity record, you must modify the End Date of the default record and set it to a date before the Start Date of the new record. This field is required. |
Copyright © 2018 General Electric Company. All rights reserved.