Deploy the SAP PI Adapters for the First Time

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic GE Digital APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

Note: This GE Digital APM module is not available in the APM Now environment.

Important: If you are using SSL, make sure you have configured SSL correctly.

StepTaskNotes
1Deploy the SAP Adapters. This step is required.
2On your SAP PI server, import the design object.This step is required.
3On your SAP PI server, import the configuration object. This step is required.
4On your SAP PI server, modify the baseline communication channels.This step is required.
5On your SAP PI server, activate the RFCReceiverToECC object.This step is required.
6

In GE Digital APM, configure the GE Digital APM system to create Notifications from Recommendation records belonging to customer-defined Recommendation families.

This step is required only if you are using the Notification Management Adapter.

7On your SAP PI server, add entries to the /MIAPM/TASK_CNF table.This step is required.
8In SAP, define the command name.This step is required.
9In SAP, install the SAPCAR file.This step is required.
10In SAP, create SAP PI directory structure.This step is required.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.