Define the Command Name in SAP

Note: If you are not using a compression method during the extraction, then you can skip this procedure.

If you are using a compression option in the context file, you need to define the command name for the compression type you are using. There are two types of compressions for APM Connect SAPCAR and ZIP. You can only use one type of compression.

Note: It is recommended to use SAPCAR as your compression type.

Steps

  1. In SAP, run the transaction code SM69.

    The External Operation System Commands screen appears.

  2. Select .

    The Create an External Command screen appears.

  3. In the Command section, in the Command Name box, enter one of the following the command names:

  4. In the Definition section, in the Operating system command box, enter one of the following systems commands:

  5. Select Save.

    The Command Name is defined.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.