Import the Design Objects

Steps

  1. Access the APM Connect installation package.
  2. Navigate to the folder that corresponds to the version of SAP PI that you are using. For example, if you are using SAP PI version 7.3, navigate to SAP PI 730.
  3. Copy the file APMConnect_DesignObjects_BaseV4.tpz.

  4. On the SAP PI Server, paste the copied file to the folder \usr\sap\<SID>\SYS\global\xi\repository_server\import, where <SID> is the system ID of the SAP PI Server.

    -or-

    Paste the copied file anywhere on your local machine.

  5. If you are using a version prior to SAP PI 7.3, select Integration Repository.

    -or-

    If you are using SAP PI 7.3 or above, select Enterprise Services Builder.

    A login screen appears.

  6. Log in as an administrator.

    Depending on the SAP PI Server version you are using, the Design: Integration Builder window or the Enterprise Services Builder window appears.

  7. On the Tools menu, select Import design objects.

    The Choose Import Source window appears.

  8. Select Client if the file copied in step 3 was pasted onto your local machine, or select Server if the file copied in Step 3 was pasted into the folder \usr\sap\<SID>\SYS\global\xi\repository_server\import on the SAP PI Server.
  9. Select the Design Objects folder.
  10. Select the file APMConnect_DesignObjects_BaseV4.tpz, and then select OK.

    A confirmation window appears.

  11. Select Import.

    The file is imported.

  12. Select Close.

    The design objects are imported and appear in the Objects section.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.