Import the Configuration Object

Steps

  1. Access the APM Connect installation package.
  2. Navigate to the folder that corresponds to the version of SAP PI that you are using. For example, if you are using SAP PI version 7.3, navigate to SAP PI 730.
  3. Copy the file APMConnect_ConfigurationObjectsV4.tpz.
  4. On the SAP PI Server, paste the copied file into the folder \usr\sap\<SID>\SYS\global\xi\directory_server\import, where <SID> is the system ID of the SAP PI Server.

    -or-

    Paste the copied file anywhere on your local machine.

  5. In a web browser, navigate to http://<SAP PI Server>:<port number>/rep/start/index.jsp, where <SAP PI Server> is the name of the SAP PI Server and <port number> is the port number of the specified SAP PI Server.

    The SAP Exchange Infrastructure window appears.

  6. Select Integration Directory.

    A login screen appears, prompting you to log in to the Configuration: Integration Builder.

  7. Log in as an administrator.

    The Configuration: Integration Builder window appears.

  8. On the Tools menu, select Import configuration objects.

    The Choose Import Source window appears.

  9. Select Client if the file copied in step three was pasted onto your local machine, or select Server if the file copied in step one was pasted into the folder \usr\sap\<SID>\SYS\global\xi\directory_server\import on the SAP PI Server.
  10. Select the Configuration Objects folder.
  11. Select the file APMConnect_ConfigurationObjectsV4.tpz, and then select OK.

    A confirmation window appears.

  12. Select Import.

    The file is imported, and a confirmation message appears.

  13. Select Close.

    The configuration object is imported, and the objects appear in the Configuration Integration Builder.

What's Next? 

Copyright © 2018 General Electric Company. All rights reserved.