Editing a Query

About this task

The Edit Query feature allows you to change query parameters such as tag name, start time, end time, and so on, in Excel. The Edit Query window that displays is based on the type of query you are editing. For example, if you want to edit a calculated query data then the Calculated Edit Query window appears.

You can use the Edit Query feature to request more data than is currently displayed or you can select an output range that does not overlap the current range. However, you cannot make the output range smaller. For example, a query edit that changes the NumberOfSamples or the Output Orientation to values that result in fewer rows or columns will not work.

Procedure

  1. Select the existing query in the Excel Sheet.
  2. From the Add-in drop-down list, select the Edit Query from the Add-In drop down list or select the icon or double select any cell which has the query formula.
    The Edit Query window appears with the existing query data.
  3. Modify the query and select OK.