About Historian Data Collectors
Many data collectors bring data into the Historian server, as listed in Supported Windows Versions for Historian Collectors.
Since installation, maintenance, and troubleshooting from a Historian perspective are essentially the same for all collectors other than the File collector, this chapter summarizes the characteristics of each and highlights their differences. It also provides a detailed description for the File collector, since it differs from the other types of collectors.

Data collectors use a specific data acquisition interface that match the data source type, such as iFIX Easy Data Access (EDA) or OPC 1.0 or 2.0 (Object Linking and Embedding for Process Control). For more information, see Supported Acquisition Interfaces. The Simulation collector generates random numeric and string data. The File collector reads data from text files.
Collector Name | Is Toolkit-Based? | Consumes a CAL? |
---|---|---|
The Calculation collector | No | Yes |
The Cygnet collector | Yes | Yes |
The File collector | No | No |
The iFIX Alarms and Events collector collector | No | No |
The iFIX collector | No | No |
The MQTT collector | Yes | Yes |
The ODBC collector | Yes | Yes |
The OPC Classic Alarms and Events collector | No | No |
The OPC Classic HDA collector | Yes | Yes |
The OPC UA DA collector | Yes | Yes |
Th OPC UA Data Access (DA) collector | No | No |
The OSI PI collector | No | No |
The Server-to-Server collector | No | Yes |
The Server-to-Server distributor | No | Yes |
The Simulation collector | No | No |
The Windows Performance collector | Yes | Yes |
The Wonderware collector | Yes | Yes |
- When failover occurs from a primary collector to a secondary collector (or vice versa), there will be some data loss as the collector tries to connect to the source to fetch the data.