Troubleshooting Historian 7.2 with PHA/PKC 6.0
Installing PHA/PKC on a machine that has Historian 7.0 or greater will fail due to a port conflict issue. Both applications use the same default port 8443. You must follow the recommended order of install below to avoid this error. Installing Historian after PHA/PKC on the same machine will not fail as Historian has the ability to detect used port and will configure an unused port.
The recommended order of install is:
- Install PHA/PKC 6.0/6.1.
- Install Historian 7.2.
Note: If you are performing an install on a system with no prior install of PHA/PKC or Historian, you must first install the Historian Alarms and Eventss Archiver and the Historian Client Tools from the Historian install media, and then you can install PHA or PKC, and then finally the rest of Historian.