Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IEnumeratedSets Interface / Unsubscribe Method
An existing set to Unsubscribe


In This Topic
    Unsubscribe Method (IEnumeratedSets)
    In This Topic
    Clear any established enumerated set subscriptions.
    Syntax
    Sub Unsubscribe( _
       ByVal enumeratedSetName As System.String _
    ) 
    void Unsubscribe( 
       System.string enumeratedSetName
    )
    void Unsubscribe( 
       System.String^ enumeratedSetName
    ) 

    Parameters

    enumeratedSetName
    An existing set to Unsubscribe
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also