Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IEnumeratedSets Interface / Rename Method
Existing set name.
New set name.


In This Topic
    Rename Method (IEnumeratedSets)
    In This Topic
    Rename an existing set in a Historian server. Renaming a set does not make the previous set name available for use.
    Syntax
    Sub Rename( _
       ByVal oldname As System.String, _
       ByVal newname As System.String _
    ) 
    void Rename( 
       System.string oldname,
       System.string newname
    )
    void Rename( 
       System.String^ oldname,
       System.String^ newname
    ) 

    Parameters

    oldname
    Existing set name.
    newname
    New set name.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also