Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / GetComments Method
An index value.


In This Topic
    GetComments Method (IDataSamples)
    In This Topic
    Return the array of data value comment records at a specific index.
    Syntax
    Function GetComments( _
       ByVal index As System.Integer _
    ) As Comment()
    Comment[] GetComments( 
       System.int index
    )
    array<Comment^>^ GetComments( 
       System.int index
    ) 

    Parameters

    index
    An index value.

    Return Value

    An array of comment records.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also