Function GetValue( _ ByVal index As System.Integer _ ) As System.Object
System.object GetValue( System.int index )
System.Object^ GetValue( System.int index )
Parameters
- index
- An index value.
Return Value
A data value.
Function GetValue( _ ByVal index As System.Integer _ ) As System.Object
System.object GetValue( System.int index )
System.Object^ GetValue( System.int index )
Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2