Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / HaveTimes Method


In This Topic
    HaveTimes Method (IDataSamples)
    In This Topic
    Whether data value times are provided.
    Syntax
    Function HaveTimes() As System.Boolean
    System.bool HaveTimes()
    System.bool HaveTimes(); 

    Return Value

    True if this instance includes data value times.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also