Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / Qualities Method


In This Topic
    Qualities Method
    In This Topic
    Return a collection of data value qualities.
    Syntax
    Function Qualities() As System.Collections.Generic.Dictionary(Of Integer,IDataQuality)
    System.Collections.Generic.Dictionary<int,IDataQuality> Qualities()
    System.Collections.Generic.Dictionary<int,IDataQuality^>^ Qualities(); 

    Return Value

    Collection of data value qualities.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also