Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IDataSamples Interface / HaveQuality Method


In This Topic
    HaveQuality Method (IDataSamples)
    In This Topic
    Whether data value qualities are provided.
    Syntax
    Function HaveQuality() As System.Boolean
    System.bool HaveQuality()
    System.bool HaveQuality(); 

    Return Value

    True if this instance includes data value qualities.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also