Add and Configure an OPC Classic Alarms and Events Collector

About this task

The OPC Classic Alarms and Events collector collects alarms and events data from any OPC 1.0 or OPC 2.0 compliant OPC server.

You can create an OPC Alarms and Events collector only for an on-premises Historian server, not for a cloud destination.

This topic describes how to add a collector instance using Configuration Hub. You can also add a collector instance using the RemoteCollectorConfigurator utility, which does not require you to install Web-based Clients.

Procedure

  1. Access Configuration Hub.
  2. In the NAVIGATION section, select Collectors.
    A list of collectors in the default system appears.
  3. If needed, select the system in which you want to add a collector instance.

  4. In the upper-right corner of the main section, select .

    The Add Collector Instance: <system name> window appears, displaying the Collector Selection section. The MACHINE NAME field contains a list of machines on which you have installed collectors.
  5. In the MACHINE NAME field, select the machine in which you want to add a collector instance.
  6. In the COLLECTOR TYPE field, select OPC Alarms and Events Collector, and then select Get Details.
    The INSTALLATION DRIVE and DATA DIRECTORY fields are disabled and populated.
  7. Select Next.
    The Source Configuration section appears.
  8. In the OPC A&E SERVER field, enter the host name or IP address of the OPC server from which you want to collect alarms and events data.
  9. Select Next.
    The Destination Configuration section appears. Under CHOOSE DESTINATION, the Historian Server option is selected by default; the other options are disabled. In addition, the DESTINATION HISTORIAN SERVER field is disabled and populated.
  10. In the USERNAME and PASSWORD fields, enter the credentials to access the destination Historian server. Values are required only for a remote Historian server.
  11. Select Next.
    The Collector Initiation section appears.
  12. If needed, modify the value in the COLLECTOR NAME field. The value must be unique.
  13. In the RUNNING MODE field, select one of the following options.
    • Service - Local System Account: Select this option if you want to run the collector as a Windows service using the credentials of the local user (that is, the currently logged-in user). If you select this option, the USERNAME and PASSWORD fields are disabled.
    • Service Under Specific User Account: Select this option if you want to run the collector as a Windows service using a specific user account. If you select this option, you must enter values in the USERNAME and PASSWORD fields.
      If you have enabled the Enforce Strict Collector Authentication option in Historian Administrator, you must provide the credentials of a user who is added to at least one of the following security groups:
      • iH Security Admins
      • iH Collector Admins
      • iH Tag Admins

    You can also configure the collector to start automatically when you start the computer.

  14. Select Add.
    The collector instance is added. The fields specific to the collector section appear in the DETAILS section.
  15. If needed, enter values in the available sections.
  16. In the upper-left corner of the page, select Save.

    The changes to the collector instance are saved.
  17. If needed, restart the collector.

What to do next

Specify the tags whose data you want to collect using the collector.