Collector Configuration - Common Fields
This topic provides a list of general fields that you can configure for any collector instance. These fields appear in the DETAILS section when you select a collector instance. For fields specific to a cloud destination, refer to Alibaba Cloud, AWS Cloud, Azure Cloud, Google Could, and Predix Cloud. For fields specific to the collector type, refer to the topics on adding and configuring each individual collector.
After you enter/modify a value in these fields, the changes are saved automatically after you place the cursor in a different field. Until the changes are saved, the values appear in bold formatting.
Field | Description |
---|---|
Collector Name | The name of the collector instance. This field is disabled. |
Collector Type | The type of the collector instance. This field is disabled. |
Description | The description of the collector instance. This field is disabled. |
Memory Buffer Size (MB) | The size of the memory buffer currently assigned to the
store-and-forward function. The memory buffer stores data during
short-term or momentary interruptions of the server connection; the disk
buffer handles long duration outages. To estimate the size you need for
this buffer, you need to know how fast the collector is trying to send
data to the server and how long the server connection is likely to be
down. With those values and a safety margin, you can compute the
required size of the buffer. The default value is 20. |
Minimum Free Space (MB) | The minimum free disk space that must be available on the computer. If the minimum space required is not available when the collector starts, the collector will shut down. |
Total Events Collected | This field is disabled. |
Total Events Reported | This field is disabled. |
Field | Description |
---|---|
Tag Prefix | The prefix that will be added to each tag that you configure for the
collector instance. This field is disabled and populated with the name
of the collector instance. This field applies to all collectors except File and Calculation collectors. |
Collection Interval Value | The interval at which the collector collects data for all the tags
configured in the collector instance.
Important: For an OPC collector, to avoid collecting redundant values when
using device timestamps, specify a collection interval that is
greater than the OPC server update rate. |
Collection Interval | The units of measure for the collection interval value. |
Collection Type | The type of the data collection:
|
Time Assigned By | Indicates whether the timestamp for the collected data is set based on the data source or the collector. For example, for an OSI PI collector, if you select Source, the timestamp of the OSI PI server is considered for the values collected by the collector. If you select Collector, the timestamp of the collector is considered. |
Field | Description |
---|---|
Collector Compression | Indicates whether you want to apply collector compression, which is a
smoothing filter to data retrieved from the data source. By ignoring
small changes in values that fall within a deadband centered around the
last reported value, only significant changes are stored in Historian,
thus consuming less archive storage space. For more information, refer to Notes on Collector and Archive Compression. |
Deadband | Indicates whether you want to apply a deadband based on the
percentage of values or on absolute values. For example, if you set
the deadband to 20% for a range of 0 to 500 engineering units, the
deadband value is 100 units, which is 50 units on each side.
Therefore, only if the difference between two values is greater than
50, they are stored in Historian. Note: If the data quality changes
from good to bad or vice versa, the values are stored in
Historian regardless of the deadband value. |
Deadband Value | The deadband value that you want to use for values collected by the
collector. Depending on whether you have selected percent or absolute,
the deadband value is determined. For example, if you want to set a deadband of 5 units on either side of a value (that is, value +/- 5), enter 10 in the Deadband Value field, and select Absolute in the Deadband field. Similarly, if you want to set a deadband of 5% on either side of a value, enter 10 in the Deadband Value field, and select Percent in the Deadband field. For more information, refer to Notes on Collector and Archive Compression. |
Compression Timeout | The time for one poll cycle for which collector compression is not
used, thus sending all the samples to Historian. This is used for a Calculation collector or Server-to-Server collector, when calculations fail, you may possibly observe collector compression (even if it is not enabled), thus producing no results or bad quality data. In such cases, you can use compression timeout, thus sending all the samples to Historian. For more information, refer to Notes on Collector and Archive Compression. |
Compression Timeout Interval | The units of measure for compression timeout. |
Spike Logic Control | Indicates whether you want to apply spike logic to tag values. When
you apply spike logic, in the event of a sudden change in tag values, a
data sample is inserted just before the spike. The timestamp of the
inserted sample is determined by your polling interval. If samples are
collected at 1 second intervals, the inserted sample's timestamp will be
1 second before the spike. This helps clearly identify the spike, and
retains a more accurate picture of the data leading up to it. For more information, refer to Spike Logic. |
Multiplier | Specifies how much larger a spike value must be than the deadband
range before the spike logic is invoked. For example, if you enter 3 in the Multiplier field, and the deadband is set to 5%, the spike logic will not be invoked until the difference between the spike value and the previously archived data point is 15% of the EGU range. |
Interval | Specifies how many samples must have been compressed before the spike logic is invoked. For example, if you enter 4 in the Interval field, and 6 values have been compressed since the last archived data sample, the spike logic will be invoked. |
Field | Description |
---|---|
Online Tag Configuration Changes | Indicates whether you want tag configuration changes to reflect immediately. If you disable this option, any tag configuration changes will reflect only after you restart the collector instance. |
Browse Source Address Space | Indicates whether you want to allow browsing for tags in the source. You may sometimes want to disable this option to reduce processing load on the collector. |
Synchronize Timestamps to Server | Indicates whether you want to adjust the timestamp of data to align
with the time setting in the Historian server. Note that this does not
change the time setting in the collector machine; it only calculates the
timestamp based on the difference between the time settings in the
server machine and the collector machine, independent of time zone or
daylight saving differences. Note:
|
Delay Collection at Startup (sec) | The duration, in seconds, after which you want the data collection to begin post tag configuration. |
Field | Description |
---|---|
Debug Mode | The debug mode for collector logs. 0 indicates normal log level,
whereas 255 indicates that debugging is enabled. Note: Leaving the debug
mode enabled for a long time consumes disk space. |
Message Compression | Indicates whether you want to apply message compression. |
Field | Description |
---|---|
Rate Output Address |
The address in the source database into which the collector writes the output of events/minute. This will help an operator (or a HMI/SCADA application) learn the performance of the collector. Values are captured once a minute. You must enter the address of a writable analog field. For example, for an iFIX collector, enter the address of an iFIX tag
in the following format: |
Status Output Address |
The address in the source database into which the collector writes the current value of its status (for example, running, stopped). This will help an operator (or a HMI/SCADA application) learn the current status of the collector. The value is updated only if the status of the collector changes. You must enter the address of a writable text field of at least eight characters. For an iFIX collector, use TX tag for the output address. Enter the
address in the following format: |
Heartbeat Output Address |
The address in the source database into which the collector writes the heartbeat signal output. Values are captured once a minute. You must enter the address of a writable analog field. For an iFIX data collector, use an iFIX tag for the output address.
Enter the address in the following format: You can program the iFIX database to generate an alarm if values are not written every minute, notifying you that the collector has stopped. |