OPC UA for MQTT Clients

The OPC UA protocol is a standard communication mechanism for transferring data between interfaces. OPC UA clients connect to the OPC UA server and collect data from UA Variables.

OPC UA is an independent open communication platform for both industrial and business application needs. The OPC UA server acts as a bridge between the IIoT devices (such as sensors, HMI software, SCADA systems, and so on) and OPC UA clients. It protects data integrity and helps in creating a scalable, reliable, and secure connection. OPC UA supports communication protocols, and also the exchanging of data between devices. Information requested by OPC UA clients is translated through the OPC UA server.

The MQTT client application is used as a two-way data communication. You can also write from OPC UA clients to MQTT clients or from IIoT devices.

After you configure MQTT Client information (that is, establishing the connections, subscriptions, and tags), the OPC UA server reads the configuration and displays the tags in a hierarchical manner. The hierarchy includes the client's name (unique per broker), topic, and the tag name within the topic. The OPC UA server reads the values of the data subscribed to by the MQTT clients. The OPC UA data is then published to OPC UA Clients.

Refer to OPC UA Settings to configure the OPC UA settings page.