OPC UA Settings
After establishing broker connections, subscriptions, and tags information, click the
overflow icon of the MQTT plugin, and then select OPC UA
Settings to connect to the OPC UA server and establish the OPC UA client
connection.

- Server
- Logging
- Security
- Certificate
- Trust List
Server

The server connection fields are populated automatically by the system. You can also change the server details as required.
Field | Description |
---|---|
PORT | The OPC UA Client port the device will use. |
NETWORK ADDRESS | The unique identification of your physical computer or a device name. |
LOGICAL HOST NAME | Host name of the server on which OPC UA is installed. |
ORGANIZATION NAME | Name of the Organization that owns the application. |
INSTANCE NAME | Information about the OPC UA client. |
ENDPOINT URL | A network location that OPC UA Client applications can use to find and connect
to an OPC UA Server. Note:
The OPC UA specific URL, it shows
as:
|
APPLICATION URL | The unique address reference on the Internet. Also, referred to as the web address. |
APPLICATION NAME | Name of the application. |
- If you modify the OPC UA server details, it is recommended to select Restart Server to establish the OPC UA server connection.
- If you want to restart the OPC UA server, select Restart Server
and then, click Yes to the Confirm
Regenerate prompt message. After successful server connection, the
following message appears.
OPC UA Server successfully restarted.
Logging

Field | Description |
---|---|
NUMBER OF LOG FILES (MAX 100) | The number of files for log backups (range is from 1 to 100). |
MAXIMUM ENTRIES PER LOG FILE | The number of entry per log file (range is from 0 to 1000000000). |
APPLICATION TRACE LEVEL | You can trace the errors or warnings to generate the trace messages. From the application trace level, you can select None, Error, Errors and Warnings, Error, Warnings and Information or, Detailed (may impact performance) as required. |
STACK TRACE LEVEL | You can trace the information about frequently used operations. The stack
trace helps to find out the debugs in an operation and to figure out the problems
for any bug generated in the operation. From the application trace level, you can select None, Error, Errors and Warnings, Error, Warnings and Information or, Detailed (may impact performance) as required. |
LOG FILE PATH | Location of the log file. <Installation Location Drive>\Program Files\Proficy\MQTTClient\Logs\OpcUaServer.log |
![]() |
Select the Optimize Log Writes check box to optimize log events, use structured logging, exclude sensitive information, and to store the data. |
Security

Use the check boxes in the Privacy and Integrity and Security Policies sections to ensure data is secured and protected from unauthorized access. Only authorized users can access the data to view and modify as per user access privileges.
Privacy and Integrity | |
ALLOW SECURE COMMUNICATION WITHOUT DATA PRIVACY (SIGNONLY) | Encryption is still used in the initial handshake. This mode is not appropriate when legal requirements prohibit the use of encryption. |
ALLOW SECURE COMMUNICATION WITH DATA PRIVACY (SIGNANDENCRYPT) | All messages are signed and encrypted. |
Security Policies | |
BASIC256SHA256 (RECOMMENDED) | For configurations that require high security. |
AES128-SHA256-RSAOAEP (RECOMMENDED - FASTEST) | For configurations that require high speed with average security. |
AES256-SHA256-RSAPSS (RECOMMENDED - MOST SECURE) | For configurations that require very high security. |
- BASIC256 and BASIC128RSA15 are deprecated due to vulnerability and theoretical issues.
- You can verify the security permissions at the following location.
<Installation Location Drive>\Program Files\Proficy\MQTTClient\ServerConfig.xml
Certificate

- Select Generate Self-signed certificate.
- A prompt message appears. Click Yes to regenerate the server
certificate.Important: All previous server settings will be removed, and new details are updated.
OPC UA certification created successfully message appears.
- Select Restart Server to use the certificate. The new server certificate details are populated in the Certificate section.
- To view the server certificate, navigate to <Install Location Drive>\Proficy\MQTTClient\UA\pkiserver\own\certs.
Trust List

The trust list will display the certificate status (trusted and rejected) and its validity
period. Use the overflow icon and select Trust to trust the
rejected certificate, or select Reject to reject the already trusted
certificate, and select Delete to delete the certificate from the
trust list.
- Select the Refresh
icon. This will load the client certificate to the Trust List table or,
- Select the Add Certificate
icon. The Import Trust Certificate dialog appears. You can then browse to the client certificate location and Trust the certificate.
After the OPC UA settings information is saved, you can select the overflow icon of the MQTT
plugin and select Publish to publish the changes to the MQTT server.
Refer to Save and Publish for more
details.