System Requirements
The following minimum requirements are needed for using Configuration Hub 2024.
Software Requirements: Supported Browsers
Only the following browsers were tested for use with Configuration Hub and iFIX: Google®
Chrome, Microsoft® Edge based on Chromium, Mozilla® Firefox, or Apple® Safari (MAC OS only).
Note: Sometimes the MAC OS cannot resolve the system name. In this
case, update the hosts file. Also, on the MAC OS, you will be required to manually install
the Configuration Hub root certificate.
Hardware Recommendations
Be aware of the following hardware recommendations:
- For Configuration Hub, it is recommended to use a display setting at 1920x1080 or better, with scaling set to 100%.
Language Support
Be aware of the following language related requirements:
- Configuration Hub cannot be installed on computers with machine names containing non-English characters.
- Configuration Hub will display the number formats and strings as they appear on SCADA or Historian Server node. Changing the browser language will not have impact on the appearance of this data.
- For the Proficy installer, when installing iFIX English with non-English Regional Settings, non-English characters are not supported for the Client ID or Client Secret fields in the installer.
Compatibility with Other Proficy Products
Several Proficy products work with Configuration Hub. The following is a general set of versions tested to work with the Configuration Hub 2024 product:
Product | Required Version |
---|---|
Proficy Authentication | 2024 |
Proficy iFIX | 2024 |
Proficy Historian | 2024 |
Operations Hub | 2024 |
MQTT Client | 2024 |
Proficy CIMPLICITY | 2024 |
Webspace | 6.2 / 2024 |
Please see the individual product IPI for more information on software and hardware requirements per product.