General Settings

The General settings allow you to define configuration options that apply to the node you want to configure. You can specify the SCADA or View node preference, the node name, the logical name, and the local node alias.

From the Navigation pane, select your node, iFIX project, and then Project Settings. Next, click Preferences. The General project settings appear at the top if the list as shown in the following figure.

The following table describes the General settings you can configure.

Field Description
Enable SCADA (uncheck to run as View node) Select this check box to use this node as a SCADA node. Clear the check box to use this node as a View node (iClient).
Node Name

Allows you to specify a unique local node name.

Node names can be up to eight characters long. They can include alphanumeric characters, but must begin with a letter. Special characters cannot be used.
Important: If modifying the iFIX node name here in Configuration Hub, after you save and publish your changes, you must restart iFIX (as a service) through Configuration Hub to view your applied changes. If the node name was modified in iFIX, and not displaying properly in this field, you must restart iFIX manually from iFIX Startup.
Logical Name

Allows you to specify a unique local node name to specify the name in your operating system's Registry.

Node names can be up to eight characters long. They can include alphanumeric characters, but must begin with a letter. Special characters cannot be used.

Use Local Node Alias

Allows you to specify a unique local node name to specify the name in your operating system's Registry.

Node names can be up to eight characters long. They can include alphanumeric characters, but must begin with a letter. Special characters cannot be used.

You must be logged in as a user in the Administrators group to change the Local Node Alias.