Starting and Stopping iFIX Projects
From the Project Panel in Configuration Hub, you can start and stop projects using the ellipsis (…) button in Project name list.
You cannot update or start iFIX with a specific Node Name from Configuration Hub. For instance, if iFIX Webspace sessions or iFIX Remote Desktop (terminal server) sessions are started, then the node name for the iFIX DefaultProject gets updated with the last run iFIX Project Node Name/SCU file. In this case, to start iFIX with a specific Node Name, you should manually start iFIX the traditional way, such as from the iFIX Startup app, instead of through Configuration Hub.
Start a Project as a Service
To start a
project:
- From the Navigation panel, select your node name to display the grid of project names.
- Select the project name you want to start, and then select the ellipsis (…)
button and then Start as Service.
A message box appears asking if you want to continue.
- Click Yes to proceed. You will then be prompted to save any open files before the process stops.
Stop a Project
To stop a project:
- From the Navigation panel, select your node name to display the grid of project names.
- Select the project name you want to stop, and then select the ellipsis (…)
button and then Stop.
A message box appears asking if you want to continue.
- Click Yes to proceed.
Troubleshooting
If you need to start iFIX with a specific node name other than the default, use the iFIX Startup app instead of Configuration Hub to start that instance.