Execute command
Execute Command executes a command in CimView
Configure the action as follows.

1 | Action type |
2 | Command |
3 | Arguments |
4 | Working directory |
5 | Run minimized |
6 | Confirmed |
7 | Message |
8 | Translate message |
1 | Action type |
Select Execute command.
2 | Command |
Enter one: Command path name, folder name, document name with a registered extension, web page reference. Click browse to open the Windows Select a Command dialog box.
3 | Arguments |
(Usually blank) Addition information used by the program
![]() |
Opens a Text Box to enter arguments. |
4 | Working directory |
Directory path to command if it is different from the screen file directory.
![]() |
Opens a Browser for Folder browser. |
5 | Run minimized |
When checked, minimizes window associated with the command.
6 | Confirmed |
When checked, Confirmed requires confirmation at runtime.
A message box will display before the action occurs requesting confirmation to proceed.
Default: Clear. Confirmation is not required.
7 | Message |
Opens a Text Box to enter a customized confirmation message.

8 | Translate message |
Check to make the customized message text available to be emitted to the selected translation file.
For more information on translation, see Translation.