Troubleshooting Scenarios

Troubleshooting Scenarios

The following topics can help you troubleshoot issues that you may have with the Rounds Pro module:

Rounds Pro InProgress Job Error

Description

When checking in a Route, the Check In As window does not respond for a long time. The server logs may show the following errors:
  • The InProgress job has not been updated
  • Error processing readings for the Route instance

Cause

The Rounds Service is not in the Running state.

Solution

Procedure

  1. Log in to the GE Digital APM server.
  2. Verify that the Rounds Service is in the Running state. If the Rounds Service is not running, do one of the following:
    1. Start the Rounds Service manually, or
    2. Reboot the server
      The Rounds Service will start as part of boot up.