Overview

Overview of the Rounds Pro Module

In industrial sectors with plant-based organizations, enterprise assets and equipment are monitored by operators at regular intervals at multiple points to ensure health and safety. The Rounds Pro module provides enhanced features to monitor the health of the assets in a plant and detect technical problems and failures with ease, thus improving the performance of assets in the plant.

Using the Rounds Pro, operators in a plant can perform inspections proactively by identifying issues and initiating preventive or remedial actions. Rounds Pro serves as a data connect between the assets in a plant and the GE Digital APM database, which helps to drive preventive and predictive maintenance of the plant.

Using Rounds Pro and the GE Digital APM Rounds Pro mobile app, installed on hand-held devices, the operator can perform the day-to-day management of tasks through routes, steps, built-in reporting, and data collection. The module helps to identify irregularities in the assets based on the data collected and enables the operators to take corrective actions.

Access the Rounds Pro Manager Page

Before You Begin

You can access the Rounds Pro Manager module from the left navigation menu under the Health option only if you are a member of the MI Rounds-Pro Admin Security Role.

You can perform various tasks on this page based on the privileges granted to the Security Groups associated to the MI Rounds-Pro Admin Security Role.

Procedure

In the module navigation menu, select Health > Rounds Pro Manager.
The Rounds Pro Manager page appears, displaying the following tabs:
  • Route Masters: Displays a list of available routes in the database with a brief description and the status of the routes.
  • Open Instances: Displays the list of open route instances that have been created from the Route Masters.
  • Instance History: Displays history of route instances that have been checked in or completed.
  • Steps: Displays a list of steps that are used to monitor assets for specific Measurement Locations.
The Rounds Pro Manager page displays an Open Dashboard link. Select the Open Dashboard link to access the Dashboard page.
Note:
  • If GE Digital APM is deployed on an on-prem environment, and you select the Open Dashboard link, the on-prem dashboard is displayed.
  • If GE Digital APM is deployed on a unified environment, and you select the Open Dashboard link, the IBI dashboard is displayed.
Based on data collected and entered in the Rounds Pro mobile app, the Dashboard page displays the following graph and charts:
  • COMPLIANCE OVERVIEW: This chart displays the percentage of routes that are due in the next 30 days, due in the next week, due today, and overdue.
  • YEAR TO DATE COMPLIANCE: This chart displays the number of route instances that are completed from the beginning of the year till date.
  • NON-COMPLIANT ROUTES: This graph displays the number of route instances that are non-compliant for different route masters. When you select a route master, the graph provides the details about the assignment of each route instance.

Access the Rounds Designer Page

Procedure

  1. Access the Rounds Pro Overview page.
  2. Select Open Designer.
    The Rounds Designer page appears, displaying the asset and measurement location hierarchy, the route and step details of an asset, and the option to create a route.

    You can use the Asset Hierarchy to browse the parent-level assets, the child-level assets, and the measurement locations.

    Example:

    • Parent-level Asset (MRD-AA-NA-Alex Airlines)
    • Child-level Asset (MRD-AAA-NA-A320-NDB)
    • Measurement location (Temperature)