Software/Firmware Downloads
This directory contains version 6.3.4 for the LEDR2 Point-to-Point Microwave Radio.
The file ledr_version634.zip contains the following files:
ledr.mpk - The binary executable which is to be loaded into the LEDR
radio using the serial FlashUtil program or over a network connection
using TFTP. Please see the release notes or the FirmwareUpgrade.txt
file for additional information concerning the software upgrade process.
ledrroot.mib - The first SNMP MIB to included when using SNMPc
ledr.mib - The first SNMP MIB to include when using an SNMP manager other
than SNMPc.
commonledr.mib - The second SNMP MIB to include.
ledrredundant.mib - The third SNMP MIB to include.
ledrsubrate.mib - The fourth SNMP MIB to include.
ledrframede1t1.mib - The fifth SNMP MIB to include.
readme_mibs.txt - Information about the order to include the SNMP MIBs.
ReleaseNotes.doc - The release notes detailing new features and
modifications to the software.
|