-------------------------------------------------------------------- Release 1.754 Software Upgrade Procedure README -------------------------------------------------------------------- DESCRIPTION: This document will describe the Release 1.754 Software Upgrade procedure to be performed on the Outdoor Units (ODUs). ================================================================= INSTRUCTIONS: The following procedure MUST be activated for each one of the Outdoor Units (ODUs, local and remote), whose Software you wish to upgrade. (1) Please make sure that you have a stable IP connection to the relevant Outdoor Unit (ODU). This may be done by activating the PING command from the DOS prompt and verifying that all requests are returned and no error is detected. (2) Activate the SwUpd.exe file and follow its instructions: (a) Click Next to start the procedure. (b) Enter the IP Address of the relevant Outdoor Unit (ODU). (c) Click Next to begin the Software Upgrade process. (d) If all is well, click Finish to complete the process. (3) After this procedure has been completed successfully, please reset the unit in order for the new Software to be loaded.