Verify a personnel aspect

Before you begin

Note:
Activities can be inserted at both the workflow and subprocess levels.

Procedure

  1. In the navigator, click Workflow > Workflows.
  2. In the Workflows list, select the resource you want to work with
    Note:
    A resource must already have been added in order to select it from this list.
  3. In the Displays panel, click Workflow Management > Workflow Editor.
  4. Click the Workflow Editor tab.
  5. Insert an activity:
    • At the workflow level:
      • From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
        Note:
        Activities can exist only between the presubprocess and postsubprocess.
    • At the subprocess level:
      • Double-click the local subprocess you want to add the activity to.
      • From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
  6. On the activity configuration panel, click Configure Method.
    The Configure Method dialog box appears, displaying a list of the available call method service providers.
  7. Double-click IPersonnel to display the list of available call methods.
  8. Click HasAspect, and then click Finish.
    The input parameters appear in the activity configuration panel.
  9. Configure the method as follows:
    1. In the Aspect Name field, enter the name of the aspect you want to verify.
    2. In the Person or Class field, click the ellipsis button, and then select a person or class.
  10. Click Save.
  11. Run the workflow, or, on the Test/Debug tab, test the workflow to ensure that your input parameters are configured correctly.