CreatePerson (IPersonnel)
Creates a new person.
Inputs | Data Type | Description |
---|---|---|
Description | String | Specifies the description of the person. |
name | String | Specifies the name of the person, used as additional identification for
informational use. Tip: If you want to create a Windows domain user, you must
enter the name value in the following format: <Fully Qualified Windows
Domain Name>\<Windows Account Name> (for example
MyDomain.MyCompany.com\RobertGray). Because the Windows account
name is not verified against the domain when creating the user, be sure to enter the
correct account name; otherwise, the user will not be able to log in to Workflow. For
more information, see Windows Domain-Based Security. |
S95 ID | String | Specifies the S95 ID of the person to create. |
Note:
In the Configure Method dialog box, click
Next to select a resource. Otherwise, in the
Inputs section of the activity configuration panel, click the
ellipsis button to select a resource.
Outputs | Description | |
---|---|---|
DirectoryResource | Returns the information related to the new person. |