Set Windows passwords to expire

One of the benefits of using Workflow with Windows security is that you can set Windows passwords to expire.

Procedure

  1. From the Start menu, click Control Panel > Administrative Tools.
  2. Double-click Local Security Policy.
    The Local Security Policy dialog box appears.
  3. Expand the Account Policies folder.
  4. Select Password Policy.
    The password policies display in the Policy list.
  5. Double-click Maximum password age.
    The Maximum password age Properties dialog box appears.
  6. In the Password will expire in field, set the number of days after which passwords expire.
  7. Click OK.