Windows Domain Users Logging into Workflow

If you are using Windows user names and passwords within Workflow security, be aware that Windows user accounts must have the policy Access this computer from the network applied under the local security policy. By default, this policy is assigned to the groups Users and Everyone on the local machine.

If the domain policy overrides the local policy settings by removing these groups, then the Windows user names and passwords will fail with insufficient rights when trying to log in to Workflow. If domain administrators want to restrict this right, then they must do one of the following tasks in order to continue to use Windows user names and passwords within Workflow:

  • Create a Domain Group that contains all the Domain Users that will be used within Workflow security, add this group to the domain policy Access this computer from the network, and deploy this policy to all machines running Workflow.
  • Add the Domain Users group to the domain policy Access this computer from the network, and then deploy this policy to all machines running Workflow.
  • Add Authenticated Users to the domain policy Access this computer from the network, and then deploy this policy to all machines running Workflow. Be aware that this group requires each user to log on to the domain at least once to be considered an authenticated user.
  • Leave at least the Users group in the domain policy Access this computer from the network. If you choose this option, be aware that the Anonymous user and the Guest user are not part of the Users group.

Updating Existing Windows Domain Users in Workflow

If you have existing Windows domain users that were created in a previous version of Workflow, and those user accounts are now associated with one or more active directory universal or global groups, the first time those users log in, whether manually or automatically, the system will update the domain information for each user and automatically remove those users from the pre-existing Windows Users group in Workflow.