Remove an equipment property aspect
Procedure
- In the navigator, click .
- In the Workflows list, select the resource you want to work with.Note:A resource must already have been added in order to select it from this list. For more information, see Add a resource to the workflow model.
- In the Displays panel, click .
- Click the Workflow Editor tab.
- Insert an activity:
- At the workflow level:
- From the Standard Activities panel, click and drag the activity you want to insert to a drop point.Note:Activities can exist only between the presubprocess and postsubprocess.
- From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
- At the subprocess level:
- Double-click the local subprocess you want to add the activity to.
- From the Standard Activities panel, click and drag the activity you want to insert to a drop point.
- At the workflow level:
- On the activity configuration panel, click Configure Method. The Configure Method dialog box appears, displaying a list of the available call method service providers.
- Double-click IEquipment to display the list of available call methods.
- Click RemovePropertyAspect, and then click Finish.The input parameters appear in the activity configuration panel.
- Configure the call method as follows:
- In the aspectName field, enter the name of the aspect you want to remove from the property.
- In the Equipment Instance or Class field, click the ellipsis button, and then select an instance or class.
- In the propertyName field, enter the name of the property whose aspect you want to verify.
- Click Save.
- Run the workflow, or, on the Test/Debug tab, test the workflow to ensure that your input parameters are configured correctly.