Manually synchronize databases

Before you begin

You must configure your reporting database before you can synchronize it with your production database.
Note:
You cannot synchronize your databases manually if there are unsaved changes to the Reporting Schedule Editor.

Procedure

  1. From the navigator, click Proficy System > Proficy System > Reporting > Default Reporting Schedule.
  2. In the Show Compatible panel, click Reporting Schedule Editor. The Default Reporting Schedule editor appears in the Workspace.
  3. In the Manual Synchronization area, click Synchronize NOW.
    If manual synchronization starts, the Feedback Zone displays a status message that manual synchronization has started. If manual synchronization fails, the Feedback Zone displays an error message.
    Note:
    The Feedback Zone does not indicate whether manual synchronization is successful. You can use the reporting database auditing tables to determine that status of a data synchronization.