Configure Workflow user password complexity rules
At any time after installation, you can use the Configure Security tool to configure Workflow user password complexity rules. Complexity rules do not affect existing passwords. However, if a user changes his password, the complexity rules will apply.
About this task
If you are upgrading from a previous version of Workflow, you must use this tool to configure the password security features. Account lockout is enabled by default during the installation process.
Important:
When you use the Configure Security tool to make changes to password security, you must re-enter and confirm the Administrator user's password before you can save your changes.
Procedure
- On the server computer, click .The Security page appears
- Select the Enforce user password complexity rules check box, then select Simple, Normal, or Advanced to determine the level of complexity for your passwords.
- Select Simple to specify that a minimum of six characters of any type must be used in user passwords.
- Select Normal to specify that a minimum of six characters, composed of at least two digits (0-9) and three letters (a-z and/or A-Z), must be used in user passwords.
- Select Advanced to configure complex password rules. Each rule is enforced separately. Valid values range from 0 (disabled) through 100.
- Click Save, and then click Exit.